I see the following sentence on the DMM section of the CC13x2 user's guide : "Only BLE and WSN Node are supported at this time. Creating new stack types is not supported." and I am wonder if support for, for example, BLE and Thread (i.e. two protocols that use concurrently the 2.4GHz antenna) will ever be available on this platform. Do you see it happening in the near future?... I know from what I read that the DMM is on a experimental stage but some hints or at least reassurance that this is indeed plausible, would help ;)
Thanks!
IAr