This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: OTA upgrade stop in between when we use Zigbee gateway with znp OTA server.

Guru 14805 points
Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK

Hello,

I am using CC2538-CC2592EMK as ZNP and ZR based on z-stack 3.0.2 and  Zigbee 3.0 gateway on Raspberry PI(ZNP over USB)

for OTA client I am using ZR switch OTA project.

For OTA server when I use ota server tool and respective ota dongle project ...The OTA upgrade process works perfectly without any issue.

But when I use Zigbee gateway as ota server OTA upgrade starts but it stops in between, that  is after some time OTA client device will request for next block but server does not give block response and then ota client will request for end image ..but for that server does not give any response.

Attached sniffer log for response.

OTA upgrade starts at  -packet 165 and server stops sending response at packet 824.

ota upgrade starts at 165and fails at 824.rar