Other Parts Discussed in Thread: CC2538, CC2652R, Z-STACK, CC2652RB
HI YK
I try the CC2530 in Zstack 3.0.2,
I meet same question of CC2538 in Zstack 3.0.1 in last year.
now:
CC2530 Coor boot OK, CC2530 EndDevice boot OK.
and can check the AssociatedDevList[0].shortAddr in Coor.
EndDevice join to coordinator OK.
But can't send message to each other.
EndDevice Send to coordinator fail.
coordinator Send to EndDevice , fail.
but sniffer can see the packet in air.
so when use the -->
"
giGenAppScreenMode = GENERIC_MAINMODE;
bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_FORMATION |
BDB_COMMISSIONING_MODE_NWK_STEERING |
BDB_COMMISSIONING_MODE_FINDING_BINDING |
BDB_COMMISSIONING_MODE_INITIATOR_TL);
"
to boot EndDevice and coordinator is wrong ??