This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LAUNCHXL-CC26X2R1: Antenna CC26X2R1

Intellectual 420 points

Replies: 3

Views: 529

Part Number: LAUNCHXL-CC26X2R1

Hi, I have some doubts about the CC26X2R1 launchpad

1. What is the range of distance of the CC2652 with the antenna board?
2. Can you have both antennas connected at the same time? (board + external UFL).
3. In case of connecting external antenna, what should be the value of C24? Or can you just weld a resistance of 0 Ohm.

Regards, 

Jose.

  • Guru 268785 points

    1) Use http://www.ti.com/tool/RF-RANGE-ESTIMATOR to make an estimate

    2) No since that would not be a 50 ohm load.

    3) Information about this is in the schematic.

     

  • In reply to TER:

    Thanks, in the schematic, capacitor C24 has no value (DNM), I don't know what value to place on the launchpad to connect the antenna

  • Guru 268785 points

    In reply to Jose Salazar:

    The note on the schematic state: "Mount either C24 or C14". The space for C14 is by default mounted, this cap can be moved to the space of C24 if the SMA connector is wanted. 

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.