• May 29, 2015

    Bluetooth low energy BLE-Stack 1.4.1 Available for Download!

    Texas Instruments is pleased to announce the immediate availability of the Bluetooth low energy BLE-Stack 1.4.1 software stack for TI’s CC2540 and CC2541 devices. The BLE-Stack 1.4.1 is available royalty-free to customers using T...
    • Mar 11, 2015

    TI adds SimpleLink Ultra-Low Power platform to Open Source Contiki OS

    Hello World! We are very happy to announce that our cc26xx port was published to Open Source Contiki OS community on Feb 25! This adds yet another TI platform to the Contiki community, from before we have great support for CC2538 . This adds Contiki s...
    • Mar 3, 2015

    Go battery-less with the New SimpleLink Ultra-Low Power Wireless Micro-controller platform! CC2650, CC2640, CC2630

    TI is expanding the SimpleLinkTM family! Following the introduction of the lowest power WiFi solution, SimpleLink WiFi CC3200 and CC3100 , TI released to the market the New SimpleLink Ultra-Low Power Wireless Microcontroller plat...
    • Jun 9, 2014

    New App note on CC2538: Power consumption measurement and optimizations using Z-stack

    Hi Z-stack fans, I am pleased to announce that we just published an application note which describes power consumption numbers and optimization settings when using Z-Stack , running on top of CC2538 device . Please see the following link for more information: http://www.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=swra456 The link provides you access to both the application note document as...
    • Apr 25, 2014

    Welcome to CC2592 - the new SimpleLink range extender for 2.4 Ghz applications

    Hi ZigBee/6Lo W PAN/TI-MAC fans, We are pleased to announce the release of the SimpleLink CC2592 device! The CC2592 is a cost-effective and high-performance RF front end for low-power and low-voltage 2.4-GHz wireless applications. The CC2592 device provides a very small size, high-output power RF design with its 4-mm × 4-mm QFN-16 package. It features a PA/LNA and provides integrated switches, matching...
    • Jan 14, 2014

    Connect your LED lighting project with the new ZigBee® Light Link™ Development Kit

    Are you considering connecting your LED lighting project for the IoT? Simplify the development process and get to market faster with TI’s new ZigBee® Light Link™ development kit A ZigBee® wirelessly connected lighting system delivers richer user interfaces, more flexible control on top of the basic on, off and dim operations and absolute flexibility to place and move switches and other controls...
    • Dec 9, 2013

    New Z-Stack Home 1.2.0 is now available for download!

    Download the latest Z-Stack Home 1.2.0 This product supports the latest ZigBee Home Automation standard and features: ZHA 1.2 certification for 38 device types (see here ) Easy-Mode commissioning ZigBee-compliant Over-The-Air update New or enhanced sample applicationsZigBee 2012, ZCP-certified core stack Energy management set (thermostat, temperature sensor, HVAC) Door lock set (door lock and...
    • Oct 20, 2011

    TI enables the Internet-of-Things with sub-1GHz 6LoWPAN solution

    TI has just recently introduced new sub-1 GHz 6LoWPAN solutions, aimed at providing a gateway for remote, low-cost wireless sensors to connect to the Internet and a wireless extension of wired IPv6 infrastructures. By operating in the sub-1GHz band, TI’s 6LoWPAN solutions offer longer wireless range at lower power levels than traditional 2.4 GHz-based 6LoWPAN offerings. The 6LoWPAN solutions support large-scale...
    • Jun 9, 2011

    Get the PurePath Wireless Headset Development Kit: CC85XXDK-HEADSET

    Are you looking to design a wireless headset? We might just have what you need! Check out the new PurePath Wireless Headset Development Kit: CC85XXDK-HEADSET and order you kit now! Development kit content: 2 x CC85XX Headset boards 2 x Battery (3.7V, 465mAh Li-ion) 1 x CC Debugger 1 x USB micro cable 1 x 3.5mm jack to 3.5mm jack cable The development kit comes pre-programmed with firmware...
    • Jun 8, 2011

    The New CC8530 PurePath™ Wireless

    The PurePath™ Wireless platform is a cost-effective and low-power solution optimized for wireless transmission of high-quality digital audio. The CC85xx includes a robust built-in wireless audio transmission protocol and can control selected external audio devices. Utilizing numerous coexistence mechanisms allows the CC85xx to avoid interfering with, or being interfered by other 2.4 GHz radio systems...
    • Jan 13, 2011

    Alektrona and Wireless Glue pass Zigbee Smart Energy profile testing

    Congratulations to Alektrona and Wireless Glue on achieveing Smart Energy certification with their products as members of the Zigbee Alliance. Both Alektrona and Wireless Glue are part of the TI Low Power RF developer network. We are pleased that all their hard work has paid off. For those of you who are interested in joining our Third party developer program. Check out the web sites: Alektrona: ...
    • Sep 17, 2010

    CC2530ZDK_ZNP_mini Call for Early Adopters .... Help us with your feedback

    Hello CC2530 FANS! We are looking for about 10-12 early adopters who have the time to look at the absolute earliest version of new ZigBee CC2530ZDK_ZNP_mini kit and collateral. Most important we need your time commitment to provide feedback for our successful launch. We would like to get your candid comments on the " out of the box " user experience. We want to make this a great "user friendly"...
    • Sep 15, 2010

    CC2530ZDK_ZNP_mini kit recommended for new designs and replacing CC2480DK

    We have placed some preliminary information on the TI website for the CC2530ZDK_ZNP_mini kit which is the recommended replacement for the CC2480DK kit. The CC2480 is not recommended for new designs because the ZigBee PRO stack will not fit on the CC2480 since it only has 128k of flash. In addition, the ZigBee profiles going forward will only iuse the latest version of ZigBee PRO. The CC2530ZDK_ZNP_mini should be...
    • Sep 9, 2010

    Z-Stack PRO/2007 2.3.1

    The TI protocol stack implementing the ZigBee PRO/2007 specification and the Smart Energy Feature Set is available for download now: http://focus.ti.com/docs/toolsw/folders/print/z-stack.html Note that the ZStack-CC2530 does support the CC2531 USB. Although the only sample application with an explicit CC2531 target build is the ZNP, two other sample apps that have an explicit CC2531 build target will be announced...
    • Nov 13, 2008

    Hello LPRF World: Check out our new CC430 Platform announced at Elektronika 2008

    TI CC430 technology and product platform was announced at Electronica today. http://www.embedded.com/products/integratedcircuits/212001671 http://www.ti.com/corp/docs/landing/cc430/index.htm?DCMP=CC430&HQS=Other+OT+cc430