This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438A + CC2267 access vai BT always stop validate_eval_package... (call #SDK_Shutdown_BL6450)

Other Parts Discussed in Thread: MSP430F5438A, BL6450, MSP430F5438, MSP430BT5190, CC2560

Dear Sirs,

I used MSP430F5438A + CC2267 to recevie 3 ANT devices, 5 I2C devices and 1 UART device.

I writed an Application to send / get(Read/Write) data from MSP430F5438A and modified sample code of Ti provied sample via BT when all device are actived.

It could work well a moment after powr on and run,  but wait few minutes, it will enters SDK_Shutdown_BL6450 function stop BT access.

I look for where enters this function, and found it will enters  "validate_eval_package" label when code stop  SDK_Shutdown_BL6450

Where can find infomration of this validate_eval_package?

 

Thanks!

 

  • Hi Corin,

    I just realized that you are using the MSP430F5438 device. Please use the MSP430BT5190 to overcome this limitation.

    Regards,

    Miguel

  • Hu Miguel,

    Thanks your reply,

    In other words, MindTree provide sample code is only use for MSP430BT5190 + CC2560, others will be happen this limitation. right?

    I also found when I access (Read/Write) via BT 14000~ 15000 times, it will stop access and shutdown BT.

    So if I'd like to use MSP430F5438A (Because I use Ti provide CC2567PAN1327ANTBT EVM, this EVM use MSP430F5438A) to replace of MSP430BT5190, what can I do?

    I also will try to use  MSP430BT5190 to verify it again.

    Thanks!

    Best regards

    Corin.

  • Hello Corin,

    Yes, the MindTree stack is only used with MSP430BT5190 + CC2560.

    Yes, you need to replace the MSP430BT5190 - that comes in the kit - in the experimenter board.

    Regards,

    Miguel