Hi,
My customer is looking to design with the CC2564MODN and they have some questions regarding the antenna design.
They are wondering if they need to use the LTA-5320-2G4S3-A1 antenna used on the reference design to pass FCC certifications. I read on the cc2564 wiki that as long as the gain of the antenna is equal or lower than the LTA, any chip antenna will pass. Can you confirm?
Also:
- What is the gain realized for LTA-5320-2G4S3-A1 in your CC2564MODN EVB? From the LTA-5320-2G4S3-A1 datasheet, I get a number “0~1 dBi”, but that may not be what you realized in your CC2564MODN EVB design for which you got your certification and hence my question.
- If instead, we are free to use any chip-antenna, what is the target gain: 0 or 1 dBi?
- There may be more than one antenna design realizable in that chip format? Are there any other criteria we need to consider while looking for options other than your approved “LTA-5320-2G4S3-A1”
They are hoping to get someone on the call to address these questions in person, as they may have additional follow up concerns. If someone would be willing to, I would be grateful.
Thanks,
Josh