Hi,
The device use this:
IC: STM32F4, CC2564B with Bluetopia stack.
IOS version 9.2.1
Iphone 4S
I need some help regarding HFRE_Open_Remote_HandsFree_Port() when the device connect for opening the remote port on the Iphone.
The function HFRE_Open_Remote_HandsFree_Port() return success and the Iphone is connected to the Bluetooth device (Bluetooth setting of IOS). But, the problem is that, the connection is successful and nothing else happens after "HFRE Open Confirmation, ID: 0x0003". There is no Control Indicator status at all and the device can't control the Call as well.
With an Android device everything is OK.
What can I do for an Iphone device?
Thanks in advance,
Denis