Hi,
With our device, we are doing very long run to verify the robustness of our BT solution, based on TI CC2564B + third party BT stack (not BT Utopia stack).This occurrence is difficult to reproduce but we have the "TI BT logger" traces for the occurrence described hereafter (unfortunately no HCI + sniffer traces)
After several hours, our device got a HCI BT disconnect event (was connected to a Phone) from the TI CC2564. In this case, our device triggers a connection attempt and the device receive HCI event negative completion with "paging timeout" (which is fine). After a few seconds, we perform a second connection attempt, but TI CC2564 does not send any HCI event about the connection state and our stack is stuck waiting a HCI event from TI CC2564.
Could you please have a look in the attached traces to check if there could be a potential issue in the TI CC2564 ?
In this thread, I have attached the 2 snapshots of the first connection attempt and the second connection attempt + the full BT logger trace containing the 2 connection attempts.
BR,
Franck