Hi everybody,
is there any way to connect TLV320AIC3100EVM-U to the system (STM32F4-DISCOVERY + CC256XQFNEM + CC256XEM-STADAPT)?
Thanks in advance
Paolo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everybody,
is there any way to connect TLV320AIC3100EVM-U to the system (STM32F4-DISCOVERY + CC256XQFNEM + CC256XEM-STADAPT)?
Thanks in advance
Paolo
Hi Paolo,
Which modes are you running the CC2564 on, master or slave? Are you using assisted or non-assisted mode?
For assisted master-mode as an audio sink, connect pins 5, 6, 7, and 8 on the CC256XQFNEM's debug header to the corresponding I2S inputs on the TLV320AIC3100EVM (TP4, TP5, TP6, TP7). Please refer to the user guide for each EVM to determine the correct pin connections.
For non-assisted master-mode as an audio sink, connect the I2S audio output pins from your STM32F4 Discovery board to the corresponding I2S inputs on the TLV32AIC3100EVM. The inputs are still TP4-TP7, and the audio data will be sent from the CC2564, to the STM32F4, to the audio CODEC.
Let me know if this helps.
Justin