I've been trying to get the example shown here processors.wiki.ti.com/index.php/CC256x_Production_Line_Testing_Guide to work but no packets are ever received.
I'm running these commands on our prototype not using the SS1Tool, but I think I'm sending the equivalent commands. No errors are returned by any of the calls on either the transmitter or the receiver. I've attached logger trace files for both the transmitter and receiver. All logs are complete from power up. We are using the AM335xBluetopiaLinuxProduction-4.0.3.0.1.0 stack.
Our BT hardware seems to be working fine as we can pair with other BT devices without a problem.
By the way there seems to be an inconsistency on the above page in the description of the HCI_VS_DRPb_Tester_Packet_TX_RX 0xFD85 command. The data in the first gray box shows shows a pattern type of 3 (f0f0) and a power level of 9. The data in the second gray box shows a pattern of 5 (PRBS9) and a power level of 15. I've tried both with the same results.
Any help would be most appreciated as I'm out of ideas of were the problem is.
Skip