Hello,
I am using SPPLEDemo from Bluetopia Stack v.4.0.2.2.
So I want to use Bluetooth LE as a serial port.
I have called the function RegisterSPPLE and the SPPLEServiceID is 3.
When I connect my notebook with Bluetooth module CC2564MODA via Bluetooth LE, there is no COM-port for this connection.
What do I have to do to create a COM-port for Bluetooth module in LE mode?