My device with CC2564C supports dual mode bluetooth.
According to TI document AVPR and BLE are exclusive, so i understand why BLE inquiry always fails when WBS is ongoing.
But the BLE inquiry still fails after wbs is stopped. Do you met the same issue? Could you help taking a look? Thanks!
The test case is as following:
1. start Classic bluetooth inquiry and BLE inquiry (the two inquiries are ok)
2.HCI_VS_AVPR_Enable 0xFD92 0x01, 0x00, 0x01, 0x0000
3.HCI_Vs_Wbs_Associate 0xFD78, 0x1
4.HCI_VS_Write_CODEC_Config 0xFD06
5.HCI Voice setting
6.Establish SCO connection (WBS, at this time the ble inquiry fails, the response code from CC2564C is "not allowed"
7.Disconnect SCO connection
7.HCI_Vs_Wbs_Disassociate 0xFD79
8.Send_HCI_VS_BLE_Enable 0xFD5B 0x01, 0x01
9. After wbs stops, the BLE inquiry still fails (the error code is "not allowed") even if "Send_HCI_VS_BLE_Enable 0xFD5B 0x01, 0x01" has been set.
If don't reset BT chip, the BLE inquiry can't recovery.