Part Number: CC2564-PAN1326
Hello, this is Tong.
I developed a Bluetooth transmitter device, and found there was a wireless transmission-missing-error.
The data loss was 3.2%.
Is this normal? Where can I find the related information?
If this is normal, I think I need to add an error-correction code.
Before fix the code, I wanted to know is this normal in wireless transmission.
Please tell me where can I find the related information.
=======================================================
Settings
=======================================================
Transmitter : PAN1326B (core: CC2564B) + MSP430F5438a
Receiver : PAN1326B + MSP430F5438a
Profile : SPP
data size in a packet : 200 byte
Transmission data rate : 400 kbps ~ 450kbps
Transmitting technique : direct UART(i.e. HCI) command control
Transmission Buffer size : 800 byte
HCI (UART) baud rate : 921.6 kbps
=====================================================
=====================================================
= Test result =
=====================================================
1. Throughput does not decreased more than 10% until 15 m distance between two BT modules.
2. In any places, error is always 3.2%.
Please, tell me any information related to BT error.(such as statistics)