I see following problem while installing the CC256x_Bluetooth_Hardware_Evaluation_Tool_V1.0_Setup.exe on Windows 7 PC:
"Windows error 2 occured while loading the JAVA VM"
This error can be avoided by starting the installation from the command prompt and running following command:
C:\<Path to EXE>CC256x_Bluetooth_Hardware_Evaluation_Too1.0_Setup.exe LAX_VM "c:\Program Files (x86)\Java\jre1.8.0_111\bin\java.exe"
Best Regards,
Shiv