Other Parts Discussed in Thread: CC2564
Tool/software: Code Composer Studio
Hello
I'm confused about command parameter of Packet Tx/Rx on cc2564.
If I command 0xFD85, 0x03, 0, 0xFF, 0, 2, 0, 27, 15, 1, 0x01FF as shown in CC256x_Testing_Guide on wiki(just frequency mode changed), it works fine.
However, when I command 0xFD85, 0x03, 0, 0, 5, 1, 0, 100, 15, 1, 0x01FF, no signal comes out.
As I understand of chart shown for the command parameter, for ACL packet type DH5, ACL packet data length can be defined up to 339.
can anyone tell me the reason why this command doesn't work?
Thanks.