Hi everyone,
I am using BHET v1.0 to upload an SP to a CC2564B device.
I placed my microprocessor in transparent mode, I start BHET and I select the file: initscripts-TIInit_6.7.16_bt_spec_4.1.bts.
I disabled "sleep mode" from BHET.
When I click on SEND button uploading process starts normally: PC sends some strings and the CC2564B reply at each one.
CC2564B replies only to the first 3 messages, after the 4th message it hangs and BHET rises a "COM port timed out" error.
Why? How can I solve?
Am I using the right SP? This seems to be the only SP available for CC2564B, is it right?
Thanks,
Alessandro