Other Parts Discussed in Thread: BLE-STACK
Hi,
I am having one existing product in which I have to add BLE functionality. For which I am looking for a module which should have everything in it and should talk with my host controller over UART. I came across the CC2650MODA.
1. Is this module has inbuilt BLE stack?
2. Do I need to build some firmware and load into this module to make it work? Is there any ready made firmware available to make the module pass through? I want to use GATT based customized profile.
As this is existing product and I am already having host controller (Quectel M66 module- 32-bit ARM7EJ-STM RISC) so I do not want to implement complete firmware in the module. Module can only be pass through.
Thanks in advanced for help.
Vishal N