hi i am sending inquiry command to cc256x but the inquiry result only contains ble devices actually i want to pait with a bluetooth 2.1 module
what should i do?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi i am sending inquiry command to cc256x but the inquiry result only contains ble devices actually i want to pait with a bluetooth 2.1 module
what should i do?
Mohammad,
I'm using CC256x EVM along with and STM32 kit as well and am not able to reproduce the issue that you're seeing. What steps are you taking when you try to send an inquiry?
In addition, which version of the chip are you using? Could you send me a copy of the printout from your console?
the hardware caluation tool was not working so i used bts transformation tool to convert the bts files to c file it had several options so i used long array option which gave me an array
i did this for three files
init script, avpr and ble arrays were generated then i copied these array to cc256X.h file in the corresponding sessions i built and programmed but now the stack is now the console is stuck on openstack() function