Hi,
I am working on CC2564B dual bluetooth module with ST32F765 device and Bluetopia_16_M4.fp_HW_FP.lib. In order to run the NoOs-SPPDemo in my project, I have to reconfigure the HCITrans.c to actual HAL driver since the demo project uses stm32f4 std. library that is not suit my STM32F765 chip. I have checked following;
- HCI usart settings,
- Slow Clock,
- BT shutdown pin
There is no mistake my activating scenario to run bluetooth chip. All timing diagrams are suitable corresponding datasheet. For example BT-SHUTDOWN rising while clock configuration is done and after that
RTS pin going high.
But when I run the code in debug mode return value of the BSC_Initialize() function is equal to -4, and for this reason SPPDemo project cannot work correctly. I have read previous comments about this topic and
check another options, too which activate the "__SUPPORT_CC256X_PATCH__" pre-processor definition in BTPSVEND.c file. But still does not work. I get same error as I mentioned above.
* Is there any Bluetopia version which is suitable for HAL library?
* Can I use this bluetopia library version "Bluetopia_16_M4.fp_HW_FP.lib" for STM32F765 Cortex M7 device?
* Is there any solution for OpenStack error ?
Can you help please, I have stuck there?
Thanks, Best Regars...