Hi:
The platform used is STM32F407VGT6 discovery+CC256XEM-STADAPT-V1.0+CC2564MODNEM_v1.0。The problem with demo being used by CC256XSTBTBLESW-v4.0.2.2-Setup in SPPDemo is that the initialization is not successful。
CC2564 RX connect STM32:PD8
CC2564 TX connect STM32:PD9
CC2564 CTS connect STM32:PD12
CC2564 RTS connect STM32:PD11
CC2564 nSHUTD connect STM32:PE14
CC2564 HAL CONSOLE_TXD connect STM32 :PA9
CC2564 HAL CONSOLE_RXD connect STM32 :PA10
the first problem:
This picture is the logical data that sends openstack when it is on power. It can be seen from the graph that the initialization of BTPS_Init (BTPS_Initialization) has been completed when STM32-CTS is high. Is it normal?
the second problem:
The device indicates that the power-up sequence is complete by asserting RTS low, which occurs up to 100 ms after nSHUTD goes high.Is the 91.68ms satisfied in the picture?