Tool/software: Linux
Hello,
1. Connected with a headset device via HF profile.
2. BLE function is enabled.
3. Receive a incoming call and accept it. At the same time SCO(WBS) channel will be initiated.
4. Before establish SCO the BLE function will be firstly disabled.
5. Then the process of establishing SCO is blocked with a about 30% reproduce rate also based on this special Sennheiser headset device more easily.
I attach air sniff & FW log, help check the cause please.
Thanks.