Other Parts Discussed in Thread: WL1837, OMAP-L138
WL1837MOD bluetooth firmware initialization hangs (no response) consistently at the first memory write of section NFC DMEM Init (regardless UART speed, tried 115200, 460800, 921600, 3000000):
#------------------ End of Platform specific Init -------------------------------
#------------------ NFC DMEM Init -----------------------------------------------
#--------------------------------------------------------------------------------
#--------------------------------------------------------------------------------
Send_HCI_VS_Write_Memory_Block 0xFF05, 0x20040300, 0x20, "03:21:76:20:C0:46:C0:46:04:22:40:1C:C0:46:C0:46:C0:46:C0:46:C0:46:C0:46:C0:46:C0:46:C0:46:C0:46"
Wait_HCI_Command_Complete_VS_Write_Memory_Block_Event 5000, 0x00, 0xff05, 0x00
The firmware is lately downloaded from TI's website, but it's the same with old version:
TIInit_11.8.32.bts
#--------------------------------------------------------------------------------
# Description : 185x/189x PG2 ROM Initialization Script
#
# Compatibility : 185x/189x 8.0.32 ROM
#
# Last Updated : 24-Jul-2018 14:40:04
#
# Version : TI_P2.143
#
#
#
#
# 185x LMP Subversion : ac8f
# 189x LMP Subversion : b08f
#
# Notes : Use this script on Diamond ROM device only (FW v8.0.32)
#--------------------------------------------------------------------------------
Appreciate for a fix on this.
By the way, why is there a NFC DMEM Init section in the script? does WL1837MOD support NFC features?
Shengchu