This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bluetooth® 5 Is Here: Top Five Questions Answered [Updated with Long Range Connections]

Guru 104615 points

Part Number: CC2640R2F, CC2642R, CC2652R, CC1352R

TI is pleased to announce general availability of the industry’s first single-mode Bluetooth® low energy production-qualified protocol stack supporting Bluetooth 5 High Speed mode (2 Mbps) as well as an evaluation SDK for developing with Long Range Connections for the SimpleLink™ CC2640R2F Bluetooth low energy wireless MCU. The SimpleLink CC2640R2 SDK 1.40, which includes the Bluetooth 5 protocol stack (BLE5-Stack) is available for immediate download at www.ti.com/tool/SIMPLELINK-CC2640R2-SDK and enables Bluetooth 5 development on the $29 CC2640R2 LaunchPad™ development kit.

This post also includes information on the newly announced SimpleLink Bluetooth 5 enabled CC1352R, CC2642R and CC2652R wireless MCUs. Please note that the CC26x2 and CC1352R devices are in pre-production status. More details about these devices and related LaunchPad development kits can be found in this post or by clicking on the product link.

The following Bluetooth 5 SDKs are available:

Bluetooth 5 (BLE5-Stack) SDK Device Features Production / Evaluation
SIMPLELINK-CC2640R2-SDK CC2640R2F High Speed (2M PHY) Production
SIMPLELINK-CC2640R2-BLE5-EVAL CC2640R2F High Speed (2M PHY)
Long Range Connections
Advertisement Extensions (AE)
Evaluation
SIMPLELINK-CC26x2-SDK CC2642R / CC2652R High Speed (2M PHY)
Long Range Connections
Advertisement Extensions (AE)
Pre-Production
SIMPLELINK-CC13x2-SDK CC1352R High Speed (2M PHY)
Long Range Connections
Advertisement Extensions (AE)
Pre-Production

Note: Production Bluetooth 5 (2 Mbps) is supported in SIMPLELINK-CC2640R2-SDK version 1.40.

We’ve put together some answers to common questions, including details on the Bluetooth 5 Throughput demo with High Speed and Long Range capability, to help enable developers to get started with Bluetooth 5 development. If you are new to Bluetooth or want to know more about the benefits Bluetooth 5, please check out our blog The secret to moving faster with Bluetooth® 5 and SimpleLink Academy.

Throughout this article, “Bluetooth” refers to Bluetooth low energy unless otherwise stated.

[Updated 23-May-17] Watch a short demonstration video of the High Speed and Long Range capability of TI's Bluetooth 5 protocol stack on Facebook here.

 

Is Bluetooth 5 backwards compatible with existing Bluetooth 4.x devices?

Yes! As with all features added in the Bluetooth 4.1, 4.2 and 5 specifications, they are optional and negotiated during the BLE connection. This ensures that Bluetooth 5 devices can reliably connect to and interact with legacy Bluetooth 4.x devices. In addition to backwards compatibility, optional features in Bluetooth 4.1 and 4.2 apply to Bluetooth 5. So, Bluetooth 5 devices may support the Data Length Extension feature from Bluetooth 4.2 in addition to the 2 Mbps feature. The TI BLE5-Stack incorporates all previous features from the existing Bluetooth 4.1 and 4.2 protocol stacks, including enhanced privacy and Secure Connections pairing.

 

How do I enable Bluetooth 5 High Speed Mode in my application?

The good news is you only need to call one new API in your application to request a BLE connection to use the 2 Mbps PHY: HCI_LE_SetDefaultPhyCmd(). This will instruct the Controller (Link Layer) to initiate what’s known as the PHY Update Procedure shown in the diagram below and is the sequence of steps that both peer devices perform to negotiate a change to the the link speed. If both devices in the connection support and prefer the 2 Mbps PHY, you’re in luck and the connection will switch over to the 2 Mbps link speed with data packets transmitted in half the time as compared to the default 1 Mbps link speed. If the peer device doesn’t support the 2 Mbps feature, or does not wish to enable it, the connection will remain at the BLE-default 1 Mbps link speed. All APIs for exchanging data (i.e., GATT) remain the same in Bluetooth 5.

We’ve put together a LE 2M PHY guide within our BLE5-Stack SW User’s Guide (SDK 1.40) with all the details on how to call this new API. Check it out here.

But wait, we’ve also enhanced our Throughput Demo on GitHub to add support for Bluetooth 5 High Speed and Long Range modes. This demo runs on two CC2640R2 LaunchPads and allows the user, via the two-button menu on the LaunchPad and a virtual serial port display to toggle between the supported PHYs while recording payload throughput and RSSI.

 


PHY Update Procedure

What range should I expect with High Speed Mode?

You may have heard that 2 Mbps connections may have “shorter range” than 1 Mbps connections. The physics behind this is quite complex, but it is true that any PHY (radio) operating in 2 Mbps mode will have 5 dB less sensitivity as compared to the PHY operating in the default 1 Mbps mode. While this may sound like a substantial loss in performance, it’s important to note that the improvements in the CC2640R2F’s radio architecture, including best-in-class RF performance, ensure high performance in personal connectivity / in-room operating environments where Bluetooth is typically used. This means you should expect greater throughput with High Speed mode at comparable distances as first generation Bluetooth 4.0 devices operating at the default LE 1 Mbps link speed.

It’s worth mentioning that another often overlooked feature in Bluetooth 5 is the Channel Selection Algorithm 2, or CSA2, that improves the BLE frequency hopping algorithm. This feature, which is supported with the TI BLE5-Stack, can reduce the impact of ‘bursty’ interference from other transmitters in the shared 2.4 GHz spectrum by ensuring that each connection event occurs at a minimum frequency offset compared to the previous connection event. Reducing packet loss from interference can reduce the number of packet retransmissions and thus improve overall energy consumption / effective throughput. Please note that the “Slot Availability Mask” feature applies to classic Bluetooth devices only and is therefore not supported by the CC2640R2F.

 

How do I evaluate Long Range BLE Connections and Advertising Extensions?

In addition to the High Speed 2 Mbps mode supported in the production BLE5-Stack v1.0.1 protocol stack which maximizes throughput with high-end Bluetooth 5 enabled smartphones that don't currently support the Long Range features of BLE5 (e.g., Samsung S8 and iPhone 8/X), TI has also enabled the ability for establishing long range connections using the LE Coded PHYs as well as broadcasting larger advertising payloads with the Advertisement Extension (AE) feature on a new CC2640R2 SDK. These new features are available in the BLE5-Stack v1.1.0 which is a component of SIMPLELINK-CC2640R2-BLE5-EVAL SDK 1.50.00.71 and allows customers to begin development and evaluations with these features that utilize the LE Coded PHYs.

The longer range in BT5 is enabled by using Forward Error Correction (FEC) to improve receiver sensitivity while transmitting at the same transmit power. If you want to know more about the science behind coded PHYs and how they improve link budget without increasing transmit power, check out our blog How does Bluetooth® 5 increase the achievable range of a Bluetooth low energy connection? which includes a video demonstration of a 1.6 km BLE Long Range connection between CC2640R2 LaunchPads.

To enable the evaluation of the LE Coded PHYs in the SDK we've updated the in box peripheral and central sample applications with ability to advertise, scan and connect on the extended advertisement channels, including with the "Long Range" LE Coded PHYs (S2 or S8).  Just program your CC2640R LaunchPads with the BLE5 simple_central & simple_peripheral then use the two-button menu provided over the LaunchPad's UART back channel to scan and connect. Updated GAP documentation is also provided in the included BLE SW User's Guide.

Please note that you cannot certify your device with Bluetooth SIG when using the LE Coded PHY evaluation configuration from this SDK or earlier SDKs.
 

What about Mesh?

Bluetooth Mesh, which was recently adopted by the Bluetooth SIG, is not part of the Bluetooth 5.0 specification. Instead, Bluetooth mesh is a standalone ("External to Core") specification that utilizes the BLE Advertising channels defined in the original Bluetooth 4.0 LE specification to 'flood' messages across the mesh network. TI intends to support Bluetooth mesh in a future product offering. To keep up on the latest status with mesh offerings from TI, we recommend subscribing for wireless connectivity updates in your myTI account.


And the rest ...


Can I use any Android 8 "Oreo" phone to evaluate this SDK with the BT5 Long Range (LE Coded PHY) feature?

Eventually, but not now. It's important to remember that Android provides a Bluetooth Host stack and interfaces with a BT/BLE Controller which is typically a separate/external chipset on these systems. The Controller implements the Link Layer and PHY layers of the BT protocol stack and interfaces to the Host using the HCI protocol over a serial bus. So, saying Android 8, which supports BT5 High Speed, AE and LE Coded PHY features means that it has the Host support (i.e., GAP) and, among other things, ability to send the relevant HCI commands to the Controller. It is perfectly valid to combine a non-BT5 equipped Controller with a BT5 enabled Host. Therefore, both the Host and Controller must both support a BT feature for it to be implemented over the air. A properly implemented BT Host will query the Controller for its locally supported features, and in this case, will only send the HCI related commands for LE Coded PHY if the Controller indicates support for such.

As of post time, we are not aware of any production BT Controllers (i.e., as typically used on mobile phone chipsets) that support the LE Coded PHY used for AE and Long Range connections. This includes the Samsung S8, iPhone 8/X, and Google Pixel 2 devices which support the BT5 High Speed feature.

 As you can see with all these great improvements Bluetooth 5 is not your father’s wireless specification. Please feel free to ask questions below.

[Updated 19-Jan-18] Details on CC26x2 and CC1352R

 

Please see the TI BLE Wiki www.ti.com/ble-wiki and sticky forum threads for additional examples & answers to most common questions!

Thank you for marking the thread as answered if your question was answered :)

54 Replies

  • In reply to JXS:

    Hello TI experts 

    I'm currently working on positioning using Bluetooth LE RSSI, for that I'm using a couple of CC2640R2 DK with BLE 4.2 stack  as a non-connectable Beacons and one DK as a scanner.  Now i would like to upgrade to BLE 5 stack,  according to what i understand regarding BLE 5 stack, the longer range feature requires a connection establishment between 2 BLE 5 nodes to be supported. My questions is: Would it be possible in the future to use the longer range feature to implement a  non-connectable Beacons to achieve longer range in the testbed?

    Thanks a lot in advance

    Mansour 

  • Guru 104615 points

    In reply to Mansour Abboud:

    Hello Mansour ,

    Yes, the Bluetooth 5 specification allows for using the LE Coded PHYs for Advertising (ADV) by way of the Advertising Extension (AE) feature. AE can be in connectable or non-connectable ADV configurations. The AE feature is currently not enabled in the BLE5-Stack v1.0.

    Best wishes

    Please see the TI BLE Wiki www.ti.com/ble-wiki and sticky forum threads for additional examples & answers to most common questions!

    Thank you for marking the thread as answered if your question was answered :)

  • In reply to JXS:

    Thanks a lot JXS) and sorry for my late replay.

    Best Reagrds

    Mansour

  • In reply to Mansour Abboud:

    Hi,

    I am able to borrow a Samsung Galaxy S8 which has Bluetooth 5.0. Can I use any BLE smartphone app to test BLE 5.0 features of my CC2640R2 Launchpad programmed with simple peripheral BLE 5?

    - kel


    Do, click "This Resolved my issue", if any of my replies helps solve your problem. For Tiva ARM Forum, see links below.

    TM4C123 NMI unlock - To those who want to use PF0 and PD7, be reminded that these pins default as NMI ! ! !

    JTAG Communication Failures

    Blog: https://markelthinkslearnscreates.wordpress.com/

    Featured Blog Projects: Bluetooth Low Energy Power Bank , Secure Internet Of Things Humidifier

    Company Projects: FOBO Tag - World’s 1st Patented Bluetooth 5 Tracker

  • In reply to Markel Robregado:

    Hi Kel

    Warning! Samsung s8 does NOT support BLE 5 PHY Long Range. We are returning our s8 after failing tests.

    Best regards,
    Jerome
  • Guru 104615 points

    In reply to JEROME H.:

    Markel Robregado - Yes, Simple Peripheral supports the PHY Update procedure for 2Mbps. I recommend using the Throughput Example from GitHub though.

    JEROME HIEBEL - Samsung does not claim support of Bluetooth 5 Long Range (LE Coded PHY) in their BT SIG end product listing: .

    As of press time, there are no Bluetooth qualified products that support the long range feature.

    Best wishes

    Please see the TI BLE Wiki www.ti.com/ble-wiki and sticky forum threads for additional examples & answers to most common questions!

    Thank you for marking the thread as answered if your question was answered :)

  • Two Questions:
    1) For the same amount of data, say 10 bytes. Is there a power difference between 1:1 bit to sample ratio verses S=8 (1:8 bit to sample ratio) ? Based on my limited understanding so far, I assume that since the TX radio will be ON for 8 times longer (in S=8) the power consumption of TX should be 8 times more for the same TX output power. Please confirm/correct
    2) Will Ti be coming out with a module for the CC2640R2F, like the one for CC2640 (CC2640MODA)? We would love to stick to Ti (currently using CC2540 and actively looking to upgrade) but we do not want to make out own module like we did the last time with CC2540.

    Thanks
    Mak
  • In reply to Noaman M:

    Hi Noaman,

    1) You are right that transferring the same amount of data will take more time with S8 coding. This will increase the total energy consumption. The current- and power consumption is however constant.

    2) As of now TI has not announced any roadmap for module(s) with CC2640R2F. There are however several 3rd party manufacturers which offers this, LSR for example: www.lsr.com/.../sable-x-ble-module

    Regards,
    Fredrik
  • In reply to Fredrik K:

    Thanks Fredrik!

    Appreciate the clarification.

    Noaman

  • How can  I realize the ble 5.0 packet sniffer with le data extension& 2mbps.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.