CC2540 module cannot run

I build module using CC2540 and success to program by flash programmer, but the software can only run when I attached the flash programmer, is there any hardware connection error , I used the circuit same as cc2540 minikit

thanks

 

1 Reply

  • Hi,

    It would be rather difficult to debug any HW issue without seeing the board design files. But some of the problems that you could be seeing, could be improper grounding, supply from the source not connected properly.

    Can you share your board design? 

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer
     button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------