What is the highest sample rate of the Sensortag Accelerometer?
How can I adjust it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to do gesture recognition and would like to know what is the highest sample rate that is supported to know If I can use TI Tag for my needs
I need sample rate of between 30-50Hz - is that possible?
user guide only talks about sample rate of magnetometer - it does not mentioned the sample rate limit on the acceleromter
Hi Ari,
I just checked by using a CC2541 USB dongle and a Sensortag v2. In this application they limited sample rate input by a lower limit of 100ms (10hz). However you can set it by editing the example code. If you are going to retrieve the sensor data through Bluetooth, as JXS mentioned earlier, fastest connection interval of BLE is 7.5ms.
when you say "this application" , which application are you referring to ?
which example code are you referring to ?
Thanks !
I tried to increase the sampling rate by changing "SENSOR_MIN_UPDATE_PERIOD" and "SENSOR_PERIOD_RESOLUTION" values.
According to the minimum connection interval (7.5ms) in theory it should be pretty easy to increase the sampling rate up to 100Hz.
but surprisingly the actual refresh rate was around 15Hz ! and it doesn't matter how high i have set the update rate.
If it is just the matter of maximum output current on the battery, Can I surmount the limitation by changing the battery ? and How?