Hello,
I am using CC2540 with input GPIO which is connected to a battery (3- 4.2 V),
currenlty i am using Zener to protect the I/O--> outcome voltage of 2.4-2.76V,I just wonder if ican change it with voltage divider,
i saw that GPIO input voltage can be Vdd+0.3V and<3.9V
Assuming that i am using voltage divider that will not exceed VDD i will have votlage from 2- 2.8 V , 2 volt is below the logic 1 input voltage ,
Bacilly it is working , shuold i change the range of the divider to have 2.4V to 3.3 or 2.5 to 3.5 , but this means input voltage on I/O will be higher than VDD...
What will be the best soultion ?