Hi,
I am using CC2650 controller and tying to write flash memory. i want to store some parameter in flash. when i ask for help in this forum i was adviced to use these functions. after trying to use thsi functions i have the following doubts
1) when writing only like FlashTest = osal_snv_write( 0x80, 28, z); where z is an array of size 28, i colud not write an array having a size >28. when lenth in this function is set to 29 or more i cant debugg or run the code.
2) when using write followed by read like
FlashTest = osal_snv_write( 0x80, 12, z);
osal_snv_read(0x80, 12, y);
Maximum size is limited to 12, if i try to increse the length more than 12 , system not working
3) when writing, data is being written to different addresses, even if i am giving the same id each time. Why ?? what is the meaning of this id value??
4) how can i erase an already written location?