Hi there,
i have the CC2650 Launchpad and i am having problem with the XDS110 Debuger.
First of all, i downloaded ther lastet CCS that is available and build my project with no error.
I also downloaded the latest embulation XDS110 packs and install under c:/ti/ccs/
So the CCS can also be updated if needed.
Than i pluged my Launchpad and saw that it runs the
Driver date: 25.11.2014
Driver Version: 1.6.0.0
So i went and aran cmd as admin on windows 64 bit and did
xdsdfu -m
xdsdfu -f firmware.bin -r
It ran with no problem and loaded the new emulation on to the XDS110 debuger.
The driver date and version are the same so i assume i have the latest installed.
Once i debug my project in to the Launchpad i got this errors messages:
Yes i did restarted CCS and Windows and got the same issues.
I also tryied to use CCS Cloud and got the same issues.
Looking at the Project propreties i have all settings done right:
So is the driver installed not the latest?
Any idea of what my cause this problem?