I am Doing OAD to simpleBLEPeripheral sample Code Provided by TI.
I followed the Process given in the OAD Guide to Produce a super HEX file which include BIM_ExtFlash+Stack+Application.
Then i used Flash Programer 2 to Load the Code into sensor Tag.
TH
>Initiate access to target: XDS-00000000. >Reading file: C:/Users/SenseGiz 1/peripheral1/SimpleBLEPeripheral/FlashOnly_ST_OAD_ExtFlash/OAD_IMAGE_FULL.hex. >Start flash erase ... >Erase finished successfully. >Start flash programming ... >Programming finished successfully. >Start flash verify ... >Skip verification of unassigned page: 0. >Skip verification of unassigned page: 10. >Skip verification of unassigned page: 11. >Skip verification of unassigned page: 12. >Skip verification of unassigned page: 13. >Page: 1 verified OK. >Page: 2 verified OK. >Page: 3 verified OK. >Page: 4 verified OK. >Page: 5 verified OK. >Page: 6 verified OK. >Page: 7 verified OK. >Page: 8 verified OK. >Page: 9 verified OK. >Page: 14 verified OK. >Page: 15 verified OK. >Page: 16 verified OK. >Page: 17 verified OK. >Page: 18 verified OK. >Page: 19 verified OK. >Page: 20 verified OK. >Page: 21 verified OK. >Page: 22 verified OK. >Page: 23 verified OK. >Page: 24 verified OK. >Page: 25 verified OK. >Page: 26 verified OK. >Page: 27 verified OK. >Page: 28 verified OK. >Page: 29 verified OK. >Page: 30 verified OK. >Page: 31 verified OK. >Verification finished successfully. >Reset target ... >Reset of target successfull.
I got this response on Uploading the Code into the Sensor tag.
I thing this means that code has been Successfully loaded.
The Problem i am facing is that The device is not Advertising. Can Someone please help me out in getting this Problem resolved.?