Tool/software: TI-RTOS
I'm getting the following error reported when running TI-RTOS -> BIOS -> Scan for errors...
Caught exception in view init code: "C:/ti/xdctools_3_32_00_06_core/packages/xdc/rov/StructureDecoder.xs", line 518: java.lang.Exception: Target memory read failed at address: 0x20003d28, length: 8
This read is at an INVALID address according to the application's section map. The application is likely either uninitialized or corrupt.
When I look at the map, this location is in the stack area.
Is this simply a stack overflow?
Do I need to allocate additional area in the stack?
Thanks,
John