Other Parts Discussed in Thread: CC2540
Hi,
I bought new CC2540 USB dongle. New installed SmartRF Packet Sniffer version 2.18.1 has no any driver for Windows 10 64-bit included. Why ?
Never mind, I have found some older driver on the E2E, which seems OK.
Bluetooth LE packets are sniffed, displayed, explained, everything seems OK.
But, may be there is some bug inside the "Display filter" function. I can successfully filter displayed packets using the field "Channel (CH)", this is OK. But any use of filter with field "Access Address (ACA)" or field "Data Type (PTY)" or field "Opcode (OPC)" generates (erroneously) only empty packet list. I did not try other fields.
Packet example:
+----------------------------------------------------+----------------- - - -
| Packet sniffer frame header |
+----+-------------+-------------------------+-------+
|info| Packet nbr. | Time stamp | Length| Packet data
+----+-------------+-------------------------+-------+----------------- - - -
| 01 | 08 00 00 00 | B4 09 DB AD 00 00 00 00 | 23 00 | 22 D6 BE 89 8E 00 17 5E 51 5C CF E5 E0 02 01 06 03 02 F0 FF 09 FF 01 04 E0 E5 CF 5C 51 5E 3F 1C EB 22 A5
+----+-------------+-------------------------+-------+----------------- - - -
Functional filter example: CH=0x25 (correct list result)
Unfunctional filter example: ACA=0x8e89bed6 (empty list result)
I have read "swru187g.pdf" with no success. Am I making some mistake ?
Thank you.
Regards, Zdenek.