Other Parts Discussed in Thread: CC2650
First, after downloading the MSP432 with simple application processor, I tried to read the data it send to the PC. But I only received "application processor Initializing" and "Done!" and didn't receive "State set to idle". Then I pressed the S1, I received nothing and can't detect the Simple AP by my phone's app. I pressed the S2, I got the data "Device being set into BSL mode" and LED2 was turned on. After a long time, there was nothing new received. The only line was "Device being set into BSL mode" and LED2 was still on. I had tried many times for this, but this problem still existed.
After that, I tried to use the XDS110 on the MSP432P401R LaunchPad to flash the BOOSTXL-CC2650MA, but it couldn't be detected by Flash Programmer 2. (I had removed all of the wire jumpers on the MSP432.)
Then I downloaded the MSP432 with Project Zero which works really well before I downloaded the simple application processor. However, now I can't detect the Project Zero by my phone's app.
What's wrong with my BOOSTXL-CC2650MA?
And how to solve these problems:
1. Not being detected by Flash Programmer 2
2.Not showing the bluetooth device (Project Zero or Simple AP)
3. BSL update didn't work.
4. "State set to idle" didn't be received after "Done!"
Thanks very much for helping me!
Jacob Guo