Other Parts Discussed in Thread: UNIFLASH, CC2650, SYSBIOS
Hi,
Trying to get some of the examples for launchxl-cc2650 working that are provided with ble_sdk_2_02_01_18
Specifically:
"\TI\simplelink\ble_sdk_2_02_01_18\examples\cc2650lp\simple_peripheral"
I can use UniFlash and download the .hex files to the board and verify that they work with BLE Scanner or similar on Android, so I know the hardware is working.
Here is my development setup:
CCS V7.3.0.00019 (Fresh install today)
TI ARM Compiler 5.2.9 (Its the closest I could find to the recommended 5.2.6 compile.
BLE SDK V2.02.01.18
CC2650 Launchpad Revision 1.2
I've imported both the cc2650lp_stack and cc2650lp_app and both compile without issue.
I download them onto the launchpad in debug mode, I can set a breakpoint in main at BIOS_Start().
Nothing happens on the PCB, and when I press pause the device is stuck in:
"ti_sysbios_family_arm_m3_Hwi_execHandler__I(...)"
Can anyone shed some light on why this is happening? More importantly how do I debug / fix this?
Thanks
Stomp!