Other Parts Discussed in Thread: CC1310,
Hi,
We are extending our work from CC1310 to CC2650 and wish to use BLE. We have used SmartRF Studio and tested the default CMD_RADIO_SETUP and CMD_FS that are generated in SmartRF on a CC2650 Launchpad.
On our firmware we use the following procedure after the radio powered:
1. Enable Clocks, PRCM Mode, Ping the RF
2. Apply any patches.
3. Start the RAT
4. Issue CMD_RADIO_SETUP, this returns Command Status = 1 (Done) and Operation Status = 0x0400 (DONE_OK)
5. Issue CMD_FS, this returns Command Status = 1(Done) and Operation Status = 0x0002 (ACTIVE).
We can never move on from the Active condition, and we can't work out why.
Can anyone suggest what might block the CMD_FS from becoming done? In a past project we have problems with CMD_FS aborting due to Silicon Revision of a CC1310, but the settings we have used are straight from SmartRF and work well using that tool.
Thanks
Stomp!