Tool/software: Code Composer Studio
Hello,
I generated a service (using bluetooth developer studio) called Voltage_Service that is meant for transmitting the voltage value as a characteristic value. The voltage was gathered by using the process in ADC single channel driver example. I attempted to pass the value of ADC0MicroVolt into the parameter using the set_parameter function (the characteristic of which had a length of 4 and the state was uint32_t.
The voltage_service shows when I connect to it via my IOS device, but whenever I try reading the value the peripheral disconnects.
Not only that, when I try accessing the other services they do not behave the way that they are supposed to.
So I guess my question is, what is the proper way to read an analog voltage and then send it over the wave through a service?