HI
My customer is working on the CC2564MODN(slave) with his NXP MCU based on the STM32 Stacks. There are some observation which we like to seek your opinion:
- After pairing done and having a power cycle(power off and on), the stack can only detect the master if the Bluetooth master is reset as well. Is there any way to have an auto pairing after a power cycle?
- Is it possible for the CC2564MODN to save the mac of two different masters and switch by firmware to connect to one of the master of choice?
- After active connection is done, if we want to do pairing with another master. Can the pairing be done straight via firmware to disconnect and pair?
INg