Using a raspberry pi to connect to CC2540. It works fine in the lab, and environments with many other advertisers.
When put in an environment that has many bluetooth advertisers, can't connect to the cc2540, or very rarely connects.
Using the bluepy library on raspberry pi.
Any advice on why the busier network blocks the connection. I was expecting that once the advertising packet was seen, a connection could be made.
Only thing I can think of is that the network is crowded, but I still expected it would make a connection.
Are there parameters in the cc2540 that make it more favorable connect; are there parameters from the master side (pi) that might be more favorable to connect.
If I get a usb plug in bluetooth module (and don't use the rapsberry pi module), is there a model that might work better.
Thanks - Jim