Other Parts Discussed in Thread: CC2650, BLE-STACK,
Tool/software: Code Composer Studio
Greetings,
I read the answer to a prior question, re: using TI Compiler V5.2.6 to compile the 'simple_peripheral' project. I just wanted to check-in with my issue to see if the answer will be the same, and ask a few more questions.
I have tried several of the CC2640R2 LaunchPad projects in the related section of 'Resource Explorer' with varying success, i.e., Project Zero loads, compiles, and is able to be discovered and manipulated. I am able to toggle both LED's. I downloaded, compiled, and ran the 'simple_broadcaster' example. While the broadcaster isn't designed to have a connection, I was still able to see it in my list of advertising BLE devices on my Android notepad. Which brings me to 'simple_peripheral'. This project I also loaded, compiled, and ran. PuTTY indicates that the system is advertising, but when I look on the notepad (running BluePixel BLE Scanner) there is *NO* indication of a BLE device advertising. I.e., it looks like a text message is being sent to PuTTY, but the device doesn't seem to actually be advertising. As mentioned, I can see and/or connect to the other projects, including connecting to my CC2650 SensorTag, so I don't think there is anything else wrong in my development chain. I am willing to add the 'other' compiler, however, before I do, is there some code inside of the 'simple_peripheral' project that can be modified ? My next step is to add/develop some i2c, RTOS, ADC code and my preference is to work across one - preferably the latest set - of tools, i.e., SCS, other modules, ....
Using CCS V7, Compiler Version TI V18.1.1.LTS, but also has V16.9.7.LTS, V16.9.6.LTS, and GNU V6.3.1
Regards,
Jim