Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
- I've built SBP demo project, FlashROM_Release configuration, and loaded it via UniFlash to a CC2642R1/CC2652R1 LaunchPads.
- The burn process completes successfully on 4(!) launch-pads (using "Load Image")
- Those four LPs run OK after the burn
- The problem - "Verify Image" fails, on all 4 LaunchPads
[4/24/2018, 3:32:17 PM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [4/24/2018, 3:32:17 PM] [WARNING] Cortex_M4_0: Warning: A firmware update is required for the debug probe. Click the "Update" button to update the firmware and connect to the debug target. DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE. (Emulation package 7.0.188.0) [4/24/2018, 3:32:17 PM] [WARNING] IcePick_C: Warning: A firmware update is required for the debug probe. Click the "Update" button to update the firmware and connect to the debug target. DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE. (Emulation package 7.0.188.0) [4/24/2018, 3:32:26 PM] [SUCCESS] IcePick_C: Warning: The firmware update completed successfully. (Emulation package 7.0.188.0) [4/24/2018, 3:32:26 PM] [SUCCESS] Cortex_M4_0: Warning: The firmware update completed successfully. (Emulation package 7.0.188.0) [4/24/2018, 3:32:27 PM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [4/24/2018, 3:32:29 PM] [INFO] Cortex_M4_0: GEL Output: Board Reset Complete. [4/24/2018, 3:32:38 PM] [SUCCESS] Program Load completed successfully. [4/24/2018, 3:33:04 PM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [4/24/2018, 3:33:06 PM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [4/24/2018, 3:33:13 PM] [ERROR] Cortex_M4_0: File Loader: Verification failed: Values at address 0x00052002 do not match Please verify target memory and memory map.
Using UniFlash 4.3.0