This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GDO0 and GDO2 pins

Other Parts Discussed in Thread: CC1101

I am having erratic communications back and forth between my access point and end point.  The success rate in getting packets through is low.  I happened to notice that when I probed the GDO0 pin with a scope, my success rate went up.  I am using SPI polling and my GDO0 and GDO2 pins are floating.  GDO0 is configured as 0x06.  Is  there anything wrong with leaving GDO0 floating when using the SPI polling method for determining packet status? Does it have to be tied through a resistor to high or low when not being used, but the IOCFG0 is configuring it to assert/deassert when packets are being received/transmitted?