As far as I can tell its not it the datasheet. I'm talking about p1_0 and p1_1.
The CC 2430 says 20ma.
If I run them in paralell can I get more?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As far as I can tell its not it the datasheet. I'm talking about p1_0 and p1_1.
The CC 2430 says 20ma.
If I run them in paralell can I get more?
Yes, you're right. It's not specified in the datasheet.
However it should be correct with 20 mA also for CC2510 too (see also this thread with the same question for CC1110 -- they all have the same I/O pads).
You were hoping to get close to 20 + 20 = 40 mA by sourcing both P1_0 and P1_1 at once, by combining them into "one" I/O pin and control them both as one I/O pin in software? I haven't tried this myself, but I suspect such a trick might work. I believe the 20 mA limit is individually per I/O pin.
Hi,
The IO pads are designed to be able to source 4 mA for the regular IOs and 20 mA for the LED IOs (P1_0 and P1_1). Regards, Richard
It's very dangerous to try to parallel them to get 40mA drive. If some bug causes only one pin to turn on then you might end up frying the chip. I'd recommend using a FET as a low side driver. I use 2N7002 a lot to drive LEDs, motors, etc. It can sink up to 300mA ,IIRC.
--Derek