Dear TI,
I am using the SmartRF04EB with SmartRF Studio 7 on a PC with windows XP SP3. When we plug the SmartRF04EB into the USB 1.1 port of the PC and start up the SmartRF Studio 7, the Smart Studio 7 will be kept at the step of finding devices as below snapshot:
Meanwhile, much CPU process is taken up by a process called startup_windows.exe as below snapshot from windows task manager. This process could not be killed and the only way is to reboot the PC:
For your addintional information
1/ The smartRF04B and smartRF studio 7 software are verified to work well on another windows 7 PC
2/ After installing smartRF studio 7 into the windows xp PC, it seems that the driver for smartRF04EB installed successfully since windows reconginizes the smartRF04B successfully as below snapshot
3/ If we start up the smartRF studio 7 without SmartRF04EB attached to the PC USB port, it will not be kept finding devices (there is no red cirle rotating left to the words "Find Device", and no startup_windows.exe to take up CPU). However, once we attach the SmartRF04EB, the problem descibed by above first picture occurs quickly.
What might be the cause for my problem here?
Thanks!
Y.M.