Hi all
I may be on a wild goose chase, but I'm trying to listen in to packets sent by an iClicker remote. It's a little 915mHz remote transceiver used in classrooms for students to send in answers to questions asked in class. The thing is, I only know a little about its transmit configuration and I'm wondering if it's possible to use SmartRF04 or a TrxEB with a CC1101EB to determine the configuration of the packets.
Here's what I know: the operating frequency is 917mHz and it uses a XE1203F transceiver chip. This chip can only do 2-FSK. Some internet sources of questionable reliability suggest more parameters, but I set the CC1101 to these and it did not work. If I was using my ham radio rig and the clicker was another ham, I'd tune to 917mHz and listen, then once I hear a chirp, I'd play with the receiver and demod until it was intelligible. Is there a way to set the 1101 "wide open" so I can do something like this? Ideally, I could start from a situation where I see the signal at 917mHz, then play with one setting (frequency shift?) until I get that right (how could I tell?), then set the next one, etc.
For this to work, there needs to be a reasonable sequence of parameters that I can run through (first do freq shift, then ...) and a way at each step to know when I've got it right. I don't know if this exists. Any suggestions would be great.
I apologize if this is called something specific that I didn't search for - I'm new to the lingo. If it is called something specific, let me know and I'll happily search for that.
Thanks!
Brian