Hi,
I'm trying to communicate a couple of CC1101 modules on WOR mode. I'm on the 433Mhz with 464kHz channel bandwidth at 1.2kbps.
I have used the settings for wor, on this link where Siri posted.
From transmitter I'm transmitting 140ms of preamble and send the data afterwards. Receiver successfully catch the packet. So no problem on catching packet. Also packet length is correct. But the real data inside the package is broken. It seems like did not successfully catch the packet bytes even though catch at correct length.
Note: As I noticed now it catches the first byte right after the length byte correctly. So in my guess, maybe somehow RX mode finishes and bytes corrupt.
What can be the cause for a situation like this? Upon your request I can supply the all settings etc.