Hello
I'm trying to make a low power transceiver for datas with a CC1120 at 450 Mhz and a Microchip Pic microcontroller.
I use a developpement kit Smart RF TRXEB texas instrument (REV 1.7.0.3).
With the Pic microcontroller connected directly to the CC1120_DK board wich is on the TRXEB board, all is OK, I can receive and transmit packets with a good power level.
After that, I made a personnal board following exactly the "450Mhz frerquency band " schematic by texas instruments, without the external osc option (I give you the link: http://www.ti.com/lit/df/tidr227/tidr227.pdf ).
On this board, there is a CC1120 embedded and a Pic microcontroller embedded (exactly the same program is running in the pic microcontroller), When I switch on the 3 Volts power, the SPI is working good because I can obtain the IDLE mode or the TX mode. But When the TX mode is actived, the CC1120 try to run in TX during 5 seconds with a high current 50 mA or more (following the TX power programmed by the SPI), and I can see a little trace on the spectrum analyser, but His power is very small, and the frequency is not good, and the packets are not transmitted. After 5 seconds, the high current stops (protection?...), and I must switch off then on the DC power to restart the system for 5 seconds.
I think there is an RF output problem on the CC1120, but I don't know what is it... Can you help me please?
Best regards from France!