Is CC430 compatible with IEEE802.15.4 standard?

Hi,

Befor I go deeper into CC430F6137 development can someone confirm/deny if it is compatible with

IEEE 802.15.4 standard (PHY)?

Unlike with other transceivers it is not specify (datasheet) that it does.

I see it supports ASK modulation, but does it have DSSS built in?

Is there a MAC stack for CC430?

Is there any progress on TI's 6LoWPAN?

Any pointers will be appreciated.

Regards

Jan

  • Hi Jan,

    No, the CC430 is not compatible with the 802.15.4 standard. It uses the same radio as the CC1101 which is not a DSSS radio. It can be used for proprietary protocols with 2-FSK, 4-FSK, GFSK, MSK or OOK.

    As far as I know, there are very few 802.15.4 radios available for the 900MHz band, even though the standard includes that band (TI doesn't have any). The 2.4GHz band is more globally available and has more bandwidth available. The standard for 900MHz uses a lower data rate for narrower bandwidth.

    For a stack you can use SimpliciTI on the CC430, which is a simple, proprietary network protocol stack from TI.

    Best,

    Russ

     

  • In reply to RF:

    Hi Russ,

     

     Thank you for that explanation.

     

    I was confused after seeing an advertisement from Sensinode about their 6LoWPAN stack running on CC430. I had an impression

    that 6LoWPAN runs on top of 802.15.4 PHY and MAC. Am I right or not necessary?

     

    As I am investigating 6LoWPAN and 802.15.4 transceivers, can I ask you what are the best 802.15.4 radio transceivers?

    I know of CC2520 from TI/Chipcon and ATRF231 from Atmel (both for 2.4GHz)

     

    Regards

    Jan

  • In reply to jan2809:

    Hi Jan,

    Sorry but I don't know much about 6LowPAN as I have never used it.

    Regarding the best 802.15.4 radios - of course TI's are the best :). I have used the CC2520 in a few projects with great success. I have looked at the Atmel radios and they look good but I have not used one in a project yet. One interesting feature I liked the looks of in the Atmel radios is the antenna diversity option. That could be a great feature for some applications.

    Good luck,

    Russ

     

  • In reply to RF:

    All, 

    TI is getting ready to release a 6LoWPAN development kit based on the CC1180 and CC430 series Sub-1GHz devices. We are in the process of finalizing the documentation and release it. You will be able to find more information about the kits at:

    http://processors.wiki.ti.com/index.php/CC-6LoWPAN

    You will find when reading the Wiki that 6LoWPAN is not fixed to any specific PHY. 6LoWPAN is just a standards based method for reducing the networking overhead of IPv6 for use in memory/speed constrained system. It is possible to run 6LoWPAN on 802.15.4 or 802.15.4g or even PLC.

    Regards,
    /TA 

     

     

     

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer
     button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • In reply to TA12012:

    Hello,

       Where is information on the CC1180?

    --Derek

    fixituntilitsbroken.blogspot.com

    Latest Post: "Fiducials in Altium"

  • In reply to Derek9531:

    Derek, 

    Please contact your local FAE or TI Sales reps for more information about the CC1180.

    /TA

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer
     button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • In reply to TA12012:

    Hi TA,

     Thanks for that info and link.

    Can you be more specific about the time-frame, is it a matter of months or weeks?

    Does the stack come with source code or binary only?

    Regards

    Jan

  • In reply to jan2809:

    Jan, 

    Thanks for your interest. We are in early adopter sampling phase now and it will be generally available in late Q1. There are two options:

    1. The CC1180 is a network processor and is used in conjunction with a separate applications processor (using simple API calls with source)
    2. The CC430x is a library in binary format where your final application can run along the network protocol.

    For both cases we have prepared examples for you get started with.

    /TA

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer
     button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • In reply to TA12012:

    Jan,

    In addition to TA's comments; the TI/Sensinode development kit will be using a early-version of 802.15.4g frame format. I.e we'll implement as much support for 802.15.4g as possible on the CC1180/CC430 HW.

    /Jonas

  • In reply to Firefighter:

    TA, Jonas,

     Good to hear that TI is taking seriously that part of Low Power RF (6LoWPAN) and thanks for all the information provided.

    I contacted my local TI people (both Sydney and Melbourne)  as advised by TA to ask for more info on CC1180, however they are struggling to find any.

    Would it be possible to pass the above mentioned documentation to them Down Under so they can pass it to me and others?

    Again, appreciate your support.

    Regards

    Jan