Hi all,
I am doing project on the wireless communication using simpliciti protocol. i am using the cc2510 mini development kit in my project.i have dowloaded the code for the simpliciti protocol for the cc2510 mini development kit from the website. i am doing some changes to the code in such a way that one of the module which is connected to the computer via DB9 connector and will send the character which is typed in the hyperterminal so that the another module receives the data and then transmitts the data back to the same module. This sender of the character will receive the character and then it again displays on the hyperterminal. i am able to display the character as it is.
so please help me in this...
Thanks & Regards,
N S S Sandeep.