The eZ430-RF2500 demo comes with various pre-built SimpliciTI libraries such as SimpliciTI EZ430RF NWK AP Library.lib, etc.
I downloaded the source code for SimpliciTI.
I changed the MAX_APP_PAYLOAD value to something other than 10, however my linker complains about a structure size mismatch within a module inside the library. This has been reported in previous posts.
Although I have the full SimpliciTI source, can someone please direct me towards an IAR project so that I can rebuild those libraries so that I don't have to try and build the sources themselves? Read note below....
Note: I realize that I can remove the library from my demo app and insert the SimpliciTI sources and rebuild that way. However, it does not build since it is missing all sorts of defines like MAX_NWK_PAYLOAD, the radio selection, etc. and there aren't clear instructions on how to rebuild this from scratch. Some of the BSP files that came with the eZ430-RF2500 demo have "CC2500" embedded in the filename. Should these be included? I could probably spend several days trying to figure all of this out, but it shouldn't be that way....
Thanks in advance