This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

simple_peer_to_peer

Hello, I've just downloaded and installed SimpliciTI 1.20, along with IAR7.60.1 to run the simple peer-to-peer example on twoCC1110f32

I followed the instructions, and loaded the code onto the devices, but the two tranceivers just don't link together.

i.e. After  initializing linking, LinkTo device keeps flashing both LED's and LinkListen 's green LED (1) is constantly on - meaning they have failed to link. I've tried this a dozen times, and they never link together.

I have given the two devices two different addresses.

but when I download the same program from my colleague they all work vwer well.

  • Now my questions are: 1,should I change the IAR to a newer version 2.if the problem is nothing with the version of IAR IDE,what the reasons can be ?what I can do for it ?

Thanks in advance

wanzeng